ADXL372 EXT_CLK - Setting of ODR & BW

Datasheet lacks block schematic describing the function of ODR and BW for use of EXT_CLK and text description on page 24 don't clarify all my questions. I have EXT_CLK with 614.4 and 460.8 kHz and I am wondering which ODR I can create out of it.

My understanding is that ODR select the time base 307.2 kHz (ODR<=3200 Hz) / 614.4 kHz (ODR=6400 Hz) and BW is just a divider (/2,/4,/8,/16,/32).

Assuming that, ODR will be constantly set to ODR = 6400 Hz setting and I will be able to divide by BW and create following combinations:

EXT_CLK 614.4 kHz, BW Setting: 3200, 1600, 800, 400, 200 Hz

EXT_CLK 460.8 kHz, BW Setting: 2400, 1200, 600, 300, 150 Hz

Are my assumptions correct?