ADXL362 offset error between modes

Hello

Is the offset error of ADXL362 is changed between measurement mode and wake-up mode ?

Our measurement reuslt shows the ottset error change between modes.

I would like to know if this is correct or there is any wrong with my use.

Condition

ADXL362 is set to the stable stage.

 X=Y= about 0G Z=1G

Result:

Output of X,Y,Z is changed to 10~20mg by changing measurement mode -> wake-up mode

Setting

ODR: 200Hz

Supply voltage :2.4V