ADcmXL3021: confusing FFT documentation

Hello,

The ADcmXL3021 datasheet revision 0 seems to have conflicting information regarding the bit settings in AVG_CNT register.

In page 23 table 20 (BASIC OPERATION -> SAMPLE RATE), the following valid settings (1 to 128x decimation factor) are listed:

However, in page 41 table 89 (USER REGISTER DETAILS -> AVG_CNT), the following settings are listed as valid:

Which one is correct? I haven't been able to try it myself against a known frequency, but based on a quick measurement the values in first table seem to produce more realistic output.

On a somewhat related note, in page 35 (USER REGISTER DETAILS -> X_BUF), the following formula is presented for transforming raw FFT buffer values to mg:

Does Number of FFT Averages refer to AVG_CNT or FFT_AVG1/FFT_AVG2 setting? Both are referred to as "FFT averages" at some point in the data sheet. I believe it should be AVG_CNT because I can't see how the actual averaging across FFT measurements could affect the output data format, however I don't want to count on it.

Best regards



.
[edited by: asdf at 10:07 AM (GMT 0) on 29 Nov 2019]