Y axis, 800Hz ODR
-5
0
1
2
-3
-1
1
0
2
2
0
2
2
0
2
1
1022
-14
-16
-11
-17
-14
-19
-12
-11
-14
-14
-11
-14
-11
-14
-14
-13
-11
-13
-13
-10
-13
-11
-15
-11
-11
-9
Hi Richard,
Sorry for the late replay. I think this is a separate issue than the misalignment issue we talked on another thread.
So did you say the external clock mode works fine with the clock derived from the uC but not the LTC6906 chip? Can you share the partial schematic and the clock waveform when using the LTC6906.
Apart from this, when using the SiT1569, can you switch the ODR to 3200Hz and see if the issue still happens, though it's 30% higher than the 307.2kHz clock. Extra care may need to be taken when running an external clock at a lower percentage of the default clock speed.
Please let me know if this works for you.
Hi Richard,
Sorry for the late replay. I think this is a separate issue than the misalignment issue we talked on another thread.
So did you say the external clock mode works fine with the clock derived from the uC but not the LTC6906 chip? Can you share the partial schematic and the clock waveform when using the LTC6906.
Apart from this, when using the SiT1569, can you switch the ODR to 3200Hz and see if the issue still happens, though it's 30% higher than the 307.2kHz clock. Extra care may need to be taken when running an external clock at a lower percentage of the default clock speed.
Please let me know if this works for you.