Post Go back to editing

ADXL1001/1002 motion indication.

Dear Miss, Mister.

I'm confused about the axix of sensitivity of your ADXL1001/1002 product.

When moving the accelerometer in the "+" direction, should i have a positive signal at the output of it (pin 30)?

When i' m pointing the accelerometer with the "+" sign to the ground (1g) i'm measuring 2.12 V

At 0g, i have 2.09V

With "+" pointing to the sky, i have 2.06V.

But, when i move the accelerometer in the direction of the "+", i'm measuring a negative pulse on the scope.

Moving in the "-" direction gives a positive one.

I,m very confused with this because we also use ST accelerometers (LIS344 for example) and their indications matches with the accelerometer motion (moving to the "+" gives a positive pulse.

Maybe i'm misinterpretating the datasheet?

Looking forward for your answer.

Best regards.

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.