ADXL 355 I2C with Waveforms

Hi all,

For my current project i'm trying to read data off the ADXL 355 with a analog discovery and the wavefoms software using the I2C protocol. As I'm new to this field i'm having a hard time interpreting the data coming from the sensor.

It seems my circuit from the ADXL to the analog discovery is functional(see photo 1 for test) i'm running Vsupply as 2.5V and i'm using 1kOhm pull up resistors. But the data I'm ressiving from the ADXL 355 is stuck at 0 g's 

To create the Pmod code i used the example found on the software for the adxl 345 and modified it.