is the adxl1001 suitable for condition monitoring?

Hello,

I want to monitor the condition of a rolling bearing. For this I want to use a mems acceleration sensor. In a first research I came across the ADXL1001. according to the data sheet it is suitable for accelerations of up to +/- 100g and has a sensitivity of about 20mV/g. the rolling bearing causes amplitudes of +/- 1g.

my questions are now:
is the adxl1001 suitable for my application?
if not, which one would you recommend?

Best regards.

Top Replies

Parents Reply Children
No Data