Max Sample Frequency for ADXL346 Inertial Sensor Development Board (EVAL-ADXL346Z-DB-ND)

I am trying to understand if you can reprogram the ADXL345 Inertial Sensor Development Board to use I higher sample frequency when logging data. The manual indicates that it comes standard at 100Hz but we would need to push the accelerometer to its max rate of 3200Hz (1600Hz BW). It would be great if we can do this on the dev board and still make use of the portability and micorSD data logging. 

Is this something we can easily do with the dev board?

Thank you