Problem for wifi example project (eval-adicup3029 with adxl362) through Crosscore embedded Studio

Hi,

I just learn to use Crossore embedded Studio (CCES) to program the code for Eval-adicup3029. And I get a wifi example (mqtt_publisher_adxl362) from the wifi software users guide (PDF fire shows at the bottom). as I follow the example the output data is unreadable. and I do not know the reason why is like that (the example also show unreadable result).

the example requires

Hardware Setup:
=============== 
Connect the PmodACL2 accelerometer to the SPI1 PMOD connector on the ADICUP3029 board. PMOD connectors are on the opposite end of the board from the power connector. The underside of the board labels which of the two  PMOD connectors is for SPI1.

The ESP8266 Wi-Fi module plugs into the P1 connector on the ADICUP3029. This example uses UART0 as the connection to the ESP8266. As a result, the following switch settings will need to be modified to route the UART signal to the Wi-Fi module. 

Switch     Position
====== ========
S2           WIFI

MQTT Broker and Subscriber Setup.

here is the code. the code that needs to add is the WifiSSID, WifiPassword, MQTTBrokerIP and MQTTbrokerPort in mqtt_pblisher_adxl362.h.

mqtt_pblisher_adxl362.c

/*****************************************************************************
 * mqtt_wifi_demo.c
 *****************************************************************************/


#include "mqtt_publisher_adxl362.h"
#include <common.h>
#include <common/adi_timestamp.h>

using namespace adi_sensor_swpack;

/* Static data */
static ADI_DATA_PACKET    			gSensorData;
static ADI_WIFI_TCP_CONNECT_CONFIG  gTCPConnect = {
													.nLinkID = ADI_WIFI_CONNECTION_ID,
													.pType = (uint8_t *) "TCP",
													.pIP   = aMQTTBrokerIp,
													.pPort =  aMQTTBrokerPort,
													.nTCPKeepAlive = ADI_WIFI_MQTT_PUBLISHER_KEEPALIVE};

static ADI_WIFI_MQTT_CONNECT_CONFIG gMQTTConnect = {
													.nLinkID = ADI_WIFI_CONNECTION_ID,
													.nVersion = ADI_WIFI_MQTT_PUBLISHER_VERSION,
													.pName = aMQTTPublisherName,
													.nMQTTKeepAlive = ADI_WIFI_MQTT_PUBLISHER_KEEPALIVE };

static ADI_WIFI_PUBLISH_CONFIG 		gPublishConfig = {
		 	 	 	 	 	 	 	 	 	 	 	 .pMQTTData = (uint8_t *) &gSensorData,
		 	 	 	 	 	 	 	 	 	 	 	 .nMQTTDataSize = sizeof(ADI_DATA_PACKET),
													 .pTopic = aMQTTTopicName,
													 .nLinkID = ADI_WIFI_CONNECTION_ID,
													 .nQos = ADI_WIFI_MQTT_PUBLISER_QOS};



/* Local Wi-Fi functions */
static void            InitWiFiConnection(void);
static void            adi_wifi_AplicationCallback(void * pCBParam, uint32_t nEvent, void * pArg);
static void			   MQTTPublishADXL(Accelerometer *pAxl);

/* Local system functions */
static void InitSystem(void);
static void Trap(void);
static void RepairConnection(void);

/*!
 * @brief      Main
 *
 * @details    Application entry point.
 *
 * @param [in] argc : Number of arguments (unused)
 *
 * @param [in] argv : Arguments (unused)
 *
 */
int main(int argc, char *argv[])
{
    ADXL362         adxl362;
    Accelerometer  *pAxl = &adxl362;
    SENSOR_RESULT   eSensorResult;

    /* Initialize the system */
    InitSystem();

    /* Open Accelerometer */
    eSensorResult = pAxl->open();

    if(eSensorResult != SENSOR_ERROR_NONE) {
        PRINT_SENSOR_ERROR(DEBUG_MESSAGE, eSensorResult);
        Trap();
    }

    /* Start measurement */
    eSensorResult = pAxl->start();

    if(pAxl->start() != SENSOR_ERROR_NONE) {
        PRINT_SENSOR_ERROR(DEBUG_MESSAGE, eSensorResult);
        Trap();
    }

	/* Publish ADXL362 accelerometer data using MQTT */
	MQTTPublishADXL(pAxl);
}

/*!
 * @brief      Application Callback
 *
 * @details    Called by the framework layer (adi_wifi_noos.c) when an event occurs.
 *
 * @param [in] pCBParam : Callback parameter (unused)
 *
 * @param [in] Event : Event of type #ADI_WIFI_AT_CMDCODE.
 *
 * @param [in] pArg : Callback argument (unused)
 *
 */
void adi_wifi_AplicationCallback(void * pCBParam, uint32_t nEvent, void * pArg)
{
	switch (nEvent)
		{
			case CMD_NONE:
				/* Read the publish Data. */
				adi_wifi_ParseSubscriberData();
				break;
			case CMD_HW_ERROR:
			{
			    break;
			}

			default:
				break;
		}

	return;
}

/*!
 * @brief      ESP8266 MQTT publisher demo using ADXL362 accelerometer data.
 *
 * @details    Publishes data over Wi-Fi to the broker.
 */
static void MQTTPublishADXL(Accelerometer *pAxl)
{
	ADI_WIFI_RESULT eResult;
    uint32_t        nTime = 0u;
    uint32_t        nPacketId = 0u;
    uint8_t         nConnectionFailFlag;

    /* Initialize the ESP8266 Wi-Fi module and establish a TCP connection */
    InitWiFiConnection();

    /* Send MQTT "CONNECT" message to broker */
    eResult = adi_wifi_radio_MQTTConnect(&gMQTTConnect);
    DEBUG_RESULT("Error connecting to the MQTT broker.\r\n", eResult, ADI_WIFI_SUCCESS);

    /* Start the ping timer to ping the MQTT broker before the keep alive expires */
    if(adi_wifi_StartTimer(ADI_WIFI_MQTT_PING_TIMEOUT, 1u) == ADI_WIFI_SUCCESS)
    {
    	DEBUG_MESSAGE("Starting to Publish\n");

		gPublishConfig.nPacketId = nPacketId;

		while(1)
		{
			nConnectionFailFlag = 0;

            /* If ping timer has expired */
            if (adi_wifi_IsTimerDone(1u) == 1u)
            {
        		/* Send MQTT "PINGREQ" message to broker to keep the connection alive. */
        		eResult = adi_wifi_radio_MQTTPing(ADI_WIFI_CONNECTION_ID);

        		/* Restart the ping timer */
        		if((adi_wifi_StopTimer(1u) == ADI_WIFI_SUCCESS) && (eResult == ADI_WIFI_SUCCESS))
            	{
        			if(adi_wifi_StartTimer(ADI_WIFI_MQTT_PING_TIMEOUT, 1u) != ADI_WIFI_SUCCESS)
                    {
        		    	DEBUG_MESSAGE("Failed to start ping timer\n");

                    }
            	}
            	else
            	{
	    	        DEBUG_MESSAGE("Failed to ping broker\n");
    		    	nConnectionFailFlag = 1;            	
    		    }
            }

           	/* If we did not fail to ping the broker, publish data */
            if(nConnectionFailFlag == 0u)
            {
            	DEBUG_MESSAGE("Publishing data..\n");

			    /* Pack the accelerometer data packet */
			    gSensorData.nPacketHeader = ADI_SET_HEADER(ADI_DATA_PACKET_TYPE, ADI_ACCELEROMETER_ID);
			    gSensorData.eSensorType = ADI_ACCELEROMETER_2G_TYPE;
			    
				/* Get timestamp */
				nTime = GET_TIME();
				memcpy(&gSensorData.aTimestamp, &nTime, 4u);

				/* Get x,y,x accelerometer data */
				pAxl->getXYZ((uint8_t*)&gSensorData.aPayload, 6u);

				/* Publish accelerometer data */
				if(adi_wifi_radio_MQTTPublish(&gPublishConfig) == ADI_WIFI_FAILURE)
				{
					nConnectionFailFlag = 1u;
				}
            }

            /* If we failed to ping the broker or failed to publish data, check the connection */
			if(nConnectionFailFlag == 1u)
			{
				DEBUG_MESSAGE("Troubleshooting failed connection..\n");
				RepairConnection();
			}

			gPublishConfig.nPacketId++;
		}
    }
}

/*!
 * @brief      Initializes the ESP8266 Wi-Fi module.
 *
 * @details    Initialize the ESP8266 Wi-Fi module and test the
 *             hardware connectivity. Try to connect to an access
 *             point and establish a TCP connection.
 */
void InitWiFiConnection(){
	ADI_WIFI_RESULT eResult;

    /* Initialize the ESP8266 Wi-Fi module */
	eResult = adi_wifi_Init(adi_wifi_AplicationCallback, NULL);
    DEBUG_RESULT("Error initializing the ESP8266 module.\r\n", eResult, ADI_WIFI_SUCCESS);

	eResult = adi_wifi_radio_TestAT();
    DEBUG_RESULT("Error testing hardware connectivity.\r\n", eResult, ADI_WIFI_SUCCESS);

	eResult = adi_wifi_radio_SetWiFiMode(1);
    DEBUG_RESULT("Error establishing a tcp connection.\r\n", eResult, ADI_WIFI_SUCCESS);

	eResult = adi_wifi_radio_DisconnectFromAP();
    DEBUG_RESULT("Error disconnecting from access point.\r\n", eResult, ADI_WIFI_SUCCESS);

	eResult = adi_wifi_radio_ConnectToAP(aWifiSSID, aWifiPassword,  NULL);
    DEBUG_RESULT("Error connecting to access point.\r\n", eResult, ADI_WIFI_SUCCESS);

	eResult = adi_wifi_radio_EstablishTCPConnection(&gTCPConnect);
    DEBUG_RESULT("Error establishing a tcp connection.\r\n", eResult, ADI_WIFI_SUCCESS);
}

/*!
 * @brief      Initializes the system
 *
 * @details    This function is responsible for initializing the pinmuxing, power service
 *             and wifi subsystem. It also initializes the realtime clock for to timestamp
 *             the outgoing sensor data packets.
 */
static void InitSystem(void)
{
    ADI_PWR_RESULT  ePwr;

    /* Explicitly disable the watchdog timer */
    *pREG_WDT0_CTL = 0x0u;

    /* Pinmux */
    adi_initpinmux();

    /* Initialize clocks */
    ePwr = adi_pwr_Init();
    DEBUG_RESULT("Error initializing the power service.\r\n", ePwr, ADI_PWR_SUCCESS);

    ePwr = adi_pwr_SetClockDivider(ADI_CLOCK_HCLK, 1u);
    DEBUG_RESULT("Error configuring the core clock.\r\n", ePwr, ADI_PWR_SUCCESS);

    ePwr = adi_pwr_SetClockDivider(ADI_CLOCK_PCLK, 1u);
    DEBUG_RESULT("Error configuring the peripheral clock.\r\n", ePwr, ADI_PWR_SUCCESS);

    /* Init timestamping */
    INIT_TIME();

    DEBUG_MESSAGE("Starting MQTT publisher Wi-Fi ADXL362 accelerometer demo application\r\n");

}

/*!
 * @brief      Troubleshoot and attempt to fix connection
 *
 * @details    This function is called if the ESP8266 has failed to communicate with the AP or broker.
 *             It will attempt to diagnose and repair the connectivity problem.
 */
static void RepairConnection()
{
    uint8_t         nConnectionStatus;

	if(adi_wifi_radio_GetConnectionStatus(&nConnectionStatus) == ADI_WIFI_SUCCESS)
	{

		switch(nConnectionStatus)
		{
			/*The  Station is connected to an AP and its IP is obtained, so try to connect to broker. */
			case 2:
			{
				/* Send MQTT "CONNECT" message to broker */
				if(adi_wifi_radio_MQTTConnect(&gMQTTConnect) != ADI_WIFI_SUCCESS)
				{
					DEBUG_MESSAGE("Failed to do MQTT Connect\n");
				}
				break;
			}
			
			/* The  Station has created a TCP or UDP transmission so you should try to publish again. */
			case 3:
				break;

			/* The TCP or UDP transmission of Station is disconnected. So try to establish a TCP
			 * connection and then connect to the broker.
			 */
			case 4:
			{
				if(adi_wifi_radio_EstablishTCPConnection(&gTCPConnect) == ADI_WIFI_SUCCESS)
				{
					if(adi_wifi_radio_MQTTConnect(&gMQTTConnect) != ADI_WIFI_SUCCESS)
					{
						DEBUG_MESSAGE("Failed to do MQTT Connect\n");
					}
				}
				else
				{
					DEBUG_MESSAGE("Failed to establish connection to broker\n");
				}
				break;
			}
			/*The  Station does NOT connect to an AP. So try to connect to the AP. */
			case 5:
			{
				if(adi_wifi_radio_ConnectToAP(aWifiSSID, aWifiPassword,  NULL) == ADI_WIFI_SUCCESS)
				{
					if(adi_wifi_radio_EstablishTCPConnection(&gTCPConnect) == ADI_WIFI_SUCCESS)
					{
						if(adi_wifi_radio_MQTTConnect(&gMQTTConnect) != ADI_WIFI_SUCCESS)
						{
							DEBUG_MESSAGE("Failed to do MQTT Connect\n");
						}
					}
					else
					{
						DEBUG_MESSAGE("Failed to establish connection to broker\n");
					}

				}
				else
				{
					DEBUG_MESSAGE("Failed to Connect to AP\n");
				}
				break;
			}
			default:
			{
				break;
			}
		}
	}
}

/*!
 * @brief      Trap function
 *
 * @details    In case of catastrophic errors this function is called to block
 *             infinitely.
 */
static void Trap()
{
    while(1);
}

mqtt_pblisher_adxl362.h

/*****************************************************************************
 * mqtt_wifi_demo.h
 *****************************************************************************/

#ifndef __MQTT_WIFI_DEMO_H__
#define __MQTT_WIFI_DEMO_H__

#include <base_sensor/adi_sensor.h>
#include <base_sensor/adi_sensor_packet.h>
#include <base_sensor/adi_sensor_errors.h>
#include <axl/adxl362/adi_adxl362.h>
#include <framework/noos/adi_wifi_noos.h>

/* Defined in pinmux.c. */
extern "C" int32_t adi_initpinmux(void);

/********************************* Wi-Fi Configuration *********************************/
/* SSID of the access point. */
uint8_t aWifiSSID[] = "Phone";

/* Password of the access point. */
uint8_t aWifiPassword[] = "00000000";

/********************************* MQTT Configuration *********************************/

/* IP address of the broker to publish to. */
uint8_t aMQTTBrokerIp[] = "172.20.10.2";

/* Port of the broker to publish to. */
uint8_t aMQTTBrokerPort[] = "1883";

/*! MQTT publisher name. */
uint8_t aMQTTPublisherName[] = "ADI_WIFI_MQTT";

/*! MQTT Topic name. This size of this string should be ADI_WIFI_MQTT_PACKET_SIZE - sizeof(ADI_DATA_PACKET) - 2u,
 *  If you want a longer topic name, increase the size of ADI_WIFI_MQTT_PACKET_SIZE.
 */
uint8_t aMQTTTopicName[] = "TOPIC_ADI_ADXL362";

/*! MQTT publish packet quality of service. */
#define ADI_WIFI_MQTT_PUBLISER_QOS                 (0u)

/*! MQTT publisher version. */
#define ADI_WIFI_MQTT_PUBLISHER_VERSION            (3u)

/*! MQTT publisher <-> broker connection keep alive timeout. */
#define ADI_WIFI_MQTT_PUBLISHER_KEEPALIVE          (7200u)

/*! Connection link id, valid id range (0-4) for multiple connections. 5 indicates single connection mode. */
#define ADI_WIFI_CONNECTION_ID                     (5u)

/*! MQTT publisher <-> broker PING command timeout. */
#define ADI_WIFI_MQTT_PING_TIMEOUT                 (ADI_WIFI_MQTT_PUBLISHER_KEEPALIVE - 1000u)

/********************************* Sensor Configuration *********************************/

/* Accelerometer instance ID. */
#define ADI_ACCELEROMETER_ID    				   (1u)

#endif /* __MQTT_WIFI_DEMO_H__ */

in addition, all the MQTT broker settings are done by following the example which is correct.  and the software MQTT.fx will be used to subscribe and receive the data(broker address and broker port are same n the mqtt_pblisher_adxl362.h).

once I subscribe to the topic, only hex format decoder can be shown which is wrong (in my opinion). and the plain text decoder shows the unreadable code which is same as the example. in addition, other decoders show the unreadable code also. 

  real situation 

 example result shows

Please help me,

Thank you in advance,

Oates

PDF

Parents Reply Children
No Data