Hi,
Im looking for a IMU unit to get roll, pitch and yaw measurements. Screening for 9 or more degrees of freedom, I could see there are 4 suggestions - ADIS 16488A, ADIS 16448, ADIS 16480 and ADIS16405, of which first 3 are of 10 degrees of freedom. Apart from the technical parameters, based on which ADIS16488A seems slightly ahead, I see that the description for each of these 3 as follows:
ADIS16488A : Tactical grade. 10 degrees of freedom inertial sensor.
ADIS16448 : Compact, precision ten degrees of freedom inertial sensor.
ADIS16480 : Ten degrees of freedom MEMS inertial sensor with dynamic orientation outputs.
Im curious to understand the differences between ADIS16488A and ADIS16480. Is it only the numbers - technical parameters? Is there any difference in what they give as output?
I see EKF is part of ADIS16480, is it also part of ADIS16488A or fusion algorithm has to be implemented externally?