ADXL355 Latch-up condition

Dear ADI support,

 

We have been using ADXL355BEZ in our condition monitoring (vibration transducer) products for a while, we’ve sold about 1000+ of them now.

 

We recently discovered that some of them fail strangely – they report a near-zero vibration (the AC part) - after experiencing a period of over-range high-frequency vibration. We initially suspects our firmware might have bugs, but after some research, we are now quite confident that it’s caused by the defects of ADXL355.

 

We know that ADXL355 has over-range protection mechanism when experiencing excessive accelerations. When activated, the output will be pulled towards midscale in order to protect itself. This is acceptable. But in some rare cases, this condition will persist even after power is re-cycled. The only way to bring the device back to normal is to tap it (or knock it, if you will) with a screwdriver or something.

 

While in latch-up condition, the ADXL355’s output consist of a fixed DC acceleration (in our two cases, it’s around -5g in x-axis. (we didn’t investigate other axis). On top of that, there’s also a high-frequency (around 1.6Khz) AC content, measured around 3.9g rms.

 

As I said previously, the condition is only cleared when external shock is applied. We did not try issuing self-test command. We’ll investigate more if you need more information. I’ll keep you up to date.

Parents
  • We have the same exact issue spanning across a considerable number of sensor nodes. We have definitively confirmed that the X/Y channels on ADXL355's are either:

    1. entirely stuck at the user set G range value

    2. intermittently stuck

    3. reporting very low vibrations whilst the Z axis is operating normally. 

    This has occurred on multiple ADXL355 sensors across multiple customer sites. The failure mode can be turned on/off repeatedly with a low transient shock ( < 8 Gs). The error does not relate at all to firmware since the failure mode was repeated using Analog's EVAL-ADICUP360 demo board. We are working with Analog Devices to resolve the issue but no resolution in sight..

    Feel free to contact me at: robert.cachro@dynapar.com

Reply
  • We have the same exact issue spanning across a considerable number of sensor nodes. We have definitively confirmed that the X/Y channels on ADXL355's are either:

    1. entirely stuck at the user set G range value

    2. intermittently stuck

    3. reporting very low vibrations whilst the Z axis is operating normally. 

    This has occurred on multiple ADXL355 sensors across multiple customer sites. The failure mode can be turned on/off repeatedly with a low transient shock ( < 8 Gs). The error does not relate at all to firmware since the failure mode was repeated using Analog's EVAL-ADICUP360 demo board. We are working with Analog Devices to resolve the issue but no resolution in sight..

    Feel free to contact me at: robert.cachro@dynapar.com

Children
No Data