Hello,
If I didn't want to use the magnetometer on the ADIS16488A, is it possible to disable it and save the power needed to operate it?
ADIS16488A
Production
The ADIS16488A iSensor® device is a complete inertial system
that includes a triaxis gyroscope, a triaxis accelerometer, triaxis
magnetometer, and pressure...
Datasheet
ADIS16488A on Analog.com
Hello,
If I didn't want to use the magnetometer on the ADIS16488A, is it possible to disable it and save the power needed to operate it?
Dear CWilson,
The magnetometer on the ADIS16488A cannot be disabled, and there are currently no plans to make a version without it.
However, have you considered the ADIS16489? It has similar performance to the ADIS16488, but without the magnetometer.
http://www.analog.com/adis16489
-Paul Kern
Product Applications Engineer
Thank you. I see 16489 is significantly more expensive. Is there something about it that commands a premium relative to the 16488?