ADXL355 external sync

Hello,

I have same questions about EXT_SYNC=01 Mode of ADXL355.

Could you please advise me  timing specification about the external sync signal? Are there any constraint about the sync signal?

According to the datasheet of ADXL355, EXT_SYNC=01 mode can be used with only a single sync pulse. Can we send only one

sync pulse for synchronization in this case? Or should we send sync pulse continuously?

Best regards,

Akira

Parents
  • Hello,

    I have the same question,

    but additionally, when the external CLK is used, and if there is possibility to send only one  external sync pulse to the 14th pin (DRDY),

    is it possible somehow to reassign this pin to get DRDY pulses after the single SYNC pulse? If yes - how?

    Now I have some number of PCBs, where pin 12 (Int1) is not connected, so I can't remap DataReady Int to Int1

    and pins 13 &14 are busy with CLK and SYNC.

    Also it would be good to see time chart for sync mode:

    External CLK chart,

    External Sync chart,

    Data Ready state chart (Is data ready after each 1024 ext_clk pulses since External Sync? Where is the better time interval for data reading to minimize the SPI/I2C activity influence to ADXL355' ADC convesion?)

    Best regards,

    Vadim

Reply
  • Hello,

    I have the same question,

    but additionally, when the external CLK is used, and if there is possibility to send only one  external sync pulse to the 14th pin (DRDY),

    is it possible somehow to reassign this pin to get DRDY pulses after the single SYNC pulse? If yes - how?

    Now I have some number of PCBs, where pin 12 (Int1) is not connected, so I can't remap DataReady Int to Int1

    and pins 13 &14 are busy with CLK and SYNC.

    Also it would be good to see time chart for sync mode:

    External CLK chart,

    External Sync chart,

    Data Ready state chart (Is data ready after each 1024 ext_clk pulses since External Sync? Where is the better time interval for data reading to minimize the SPI/I2C activity influence to ADXL355' ADC convesion?)

    Best regards,

    Vadim

Children
No Data