Post Go back to editing

New Article on Optimizing MEMS Gyroscope Performance!

Just a quick reference to a newly released article:

 

TITLE:

Anticipating and Managing Critical Noise Sources in MEMS Gyroscopes

 

ABSTRACT:

When a MEMS inertial measurement unit (IMU) is operating as a feedback sensor in a motion control system, gyroscope noise is an important behavior to understand because it can cause undesirable physical motion on the platform it is monitoring. Depending on the conditions, there are a number of potential error sources to consider when developing early, application-targeted noise estimates for a particular MEMS IMU. Three common gyroscope attributes to consider in this process are its inherent noise, response to linear vibration and misalignment errors. Figure 1 provides a simple model, which displays several attributes that are influential in evaluating each error source: source, sensor response, and filtering. This model provides the baseline for spectral analysis of each of these attributes.

 

LINK:

http://www.analog.com/media/en/technical-documentation/technical-articles/Anticipating-and-Managing-Critical-Noise-Sourc…

 

I hope that this helps!

NevadaMark