Post Go back to editing

EVAL ADXL354BZ. 

I bought the evaluation board EVAL ADXL354BZ last week and this is the first time to try it. 

I connected ground and power (2.7 V) in the P1 header. Connected both jumpers (Range and Mode) such that the middle pin is connected to VDDIO to have the accelerometer be in the measurement mode. Is getting zero output for the X,Y,Z and temperature.  When I switch the jumpers Mode jumper to ground, to go to standby, I get the same thing.

 

The measured voltages are as follows: VDDIO = about 1.2 V, V1P8DIG and VIP8ANA = about 2 V, ST1, ST2=0.

How do I get an output from X,Y,Z and TEMP?

Parents Reply Children
No Data