I am trying to interface a IMU ADIS16362 with a Raspberry Pi 3 board and need to know if I can directly connect the sensor to Pi SPI pins? (Pi GPIOs are 3.3V).
In the datasheet of ADIS16362 on page 4, there is a following footnote for logic inputs and digital outputs.
"The digital I/O signals are driven by an internal 3.3 V supply and the inputs are 5 V tolerant."
Does this imply that I can safely connect the IMU with 5V supply to Raspberry Pi 3.3V SPI directly?
I don't want to damage my Pi board at this point!