Article ADIS16228 Demonstration, Compressor Case

Q:

Do you have any examples for using the ADIS16228 Evaluation Software and Tools?

--------------------------------------------------------------------------------------------------------------------------

A:

Yes, here is a simple example, which involved measuring the vibration on the case of a compressor. In this example, we taped the ADIS16228/PCBZ to the top of the compressor, used a ribbon cable (6 inches) to connect it to J1 on the ADISUSBZ. The video provides a quick overview of the application and the three pictures represent the FFT output from the ADIS16228, when the compressor was off, when it was idling and when it was fully operational. From these pictures, one can easily see the difference in vibration on the compressor's case.

Figure 1. Compressor Completely Off

Figure 2. Compressor Idling

Figure 3. Compressor On

The following video shows the actual compressor.

COMING SOON:

  1. Cursor demonstration to identify the magnitude, FFT bin and center frequency of the vibration components
  2. Illustrate the impact of the FFT averaging
  3. Demonstrate the Spectral Alarms

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.