ADIS16460: FAQ

Was this helpful?
  • ADIS16460 Data Ready During Start-up

    The ADIS16460's data ready signal provides a pulse, every time that new data loads into its output data registers. By changing states while the actual register update is happening, the data-ready provides…
  • ADIS16460 Datasheet Error - SYNC_SCAL Equation/Boundary Condition

    DATASHEET ADIS16460 REVISION B LOCATION OF ERROR Page 21, second column, ~50% down from the top DATASHEET LINK http://www.analog.com/media/en/technical-documentation/data-sheets…
  • ADIS16460 Datasheet Error: Delta-Velocity Data Format Examples

    PRODUCT ADIS16460 REVISION B LOCATION OF ERROR Table 35, page 17 DATASHEET LINK http://www.analog.com/media/en/technical-documentation/data-sheets/ADIS16460.pdf#Page=17 …
  • ADIS16460 Datasheet: Accelerometer VRW?

    The Velocity Random Walk (VRW) parameter for the accelerometers, is listed incorrectly in Table 1 of the ADIS16460 datasheet (revision 0). Please see the following graphic for the correction that will…
  • ADIS16460 Datasheet: Burst-read structure?

    The description for the burst read function, located on page 11 of the ADIS16460 datasheet (revision 0), has several errors in it. Please see the following graphic for the corrected description that will…
  • ADIS16460 Datasheet: Checksum value in Burst Read?

    The present version of the ADIS16460 datasheet (revision 0) says that there is a CRC-16 code included in the burst-ready sequence. This is not correct. The "check code" is actually a checksum. Please see…
  • ADIS16460 Datasheet: Data Invalid Time

    I just found an issue with the ADIS16460 datasheet (revision 0), which relates to the Data Invalid Time in Table 2 (page 5) SOURCE: http://www.analog.com/media/en/technical-documentation/data-sheets…
  • ADIS16460 Datasheet: Gyro Resonant Frequency?

    In the ADIS16460 datasheet, revision 0, the resonant frequency parameter for the gyroscopes is listed incorrectly in Table 1. Please see the following image to see the correction, which will be in revision…
  • ADIS16460 Datasheet: Software Reset Time?

    Table 44, in the ADIS16460 datasheet (revision 0) has an error in the software reset time. Please see the following graphic for the correct information, which will also be in the next revision of the ADIS16460…
  • ADIS16460 Evaluation Hack

    For those of your who have evaluated the ADIS16334/PCBZ, ADIS16445/PCBZ or ADIS16448/PCBZ, you have an extra tool available for evaluating the newly released ADIS16460 on your EVAL-ADIS system. If you…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.