ADIS16448: FAQ

Was this helpful?
  • ADIS16448 Code Examples

    Q: Do you have any starter code for working with the ADIS16448 ? A: ------------------------------------------------------------------------------------------ Yes, we do. The ADIS16448 operates…
  • ADIS16448 Connector-Down Design

    Q: Outside of the example in the datasheet, do you have any other ideas or information that illustrate the ADIS16445 and ADIS16448 in connector-down configurations? -------------------------------…
  • ADIS16448 CRC-16 Code

    Q: Do you you have any code examples for calculating the new CRC-16 option in the ADIS16448? -------------------------------------------------------------------------------------------------------…
  • ADIS16448 Data Ready Signal During Start-up

    Q: What does the ADIS16448's data-ready signal do during start-up? ----------------------------------------------------------------------------------------------- A: Please see the attached file…
  • ADIS16448 Data Sampling

    Q: Can you offer more information on the sampling of sensor data in the ADIS16448? A: The gyroscopes, accelerometers, and temperature sensors are all sampled through a common ADC channel, which uses…
  • ADIS16448 Evaluation Tool Overview

    Q: Where do I find information on evaluation tools for the ADIS16448 Inertial Measurement Unit (IMU)? ----------------------------------------------------------------------------------------------…
  • ADIS16448 Flex Connector Supplier

    Q: Where can I purchase the flex connector for connecting the ADIS16448AMLZ to the EVAL-ADISZ ? A: -----------------------------------------------------------------------------------------------…
  • ADIS16448 Input Clock on EVAL-ADIS

    Q: How do I use an input clock to drive sampling in the ADIS16448 , when I am using the EVAL-ADIS to evaluate it? A: -----------------------------------------------------------------------------…
  • ADIS16448 Start-up Current Demand

    Q: Does the ADIS16448 have similar start-up transients as the ADIS16488A? ----------------------------------------------------------------------------------------------------------- A: The start…
  • ADIS16448 without packaging

    Question We are seeking a sensor similar to the ADIS16448, but without the pressure sensor and housing, to allow for higher integration. The module must be still functional after an acceleration of…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.