ADIS16365: FAQ

Was this helpful?
  • ADIS16365 Evaluation Tool Overview

    Q: Where do I find information on evaluation tools for the ADIS16365 inertial measurement unit (IMU)? ----------------------------------------------------------------------------------------------…
  • ADIS16365 sensitivity

    Question Is it posible to Change the Dynamic Range of the Accelerometer to enhance the Sensitivity on the ADIS16365 ? For +-18g it is 3.33 mg/LSB. We need a better Resolution but not that high…
  • ADIS16365 Static error

    Question Because they still have not got the sample, so he have to use the part (whose X axis was damaged) to do the other test. he found the Static error is quit large (Please see attached). Is that…
  • SMPL_PRD setting of ADIS16365

    Question The following customer of China meets a problem when setting the SMPL_PRD register. It’s said from datasheet that SPI clock shouldn’t be faster than 300KHz if want to set it into “low power…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.