ADIS16364: FAQ

Was this helpful?
  • ADIS16364 EVB

    Q 1. For ADIS16364, it is Factory Temperature Calibrated, so what purpose is the temperature Sensor? 2. For ADIS16364, If I put ADIS16364 on the table in static state, the output data is 0.1~1.5degree…
  • ADIS16364 not working on EVAL-ADIS

    Q: When I connect my ADIS16364 device to the EVAL-ADIS system, the gyroscopes are all pegged to 409 deg/sec and the device does not seem to be working. Any ideas? ---------------------------------…
  • ADIS16364: The purpose of temperature Sensor

    Q For ADIS16364, it is Factory Temperature Calibrated, so what purpose is the temperature Sensor? A The ADIS16364 is calibrated from -20 to +70C. The temperature sensor can provide a rough measurement…
  • Interface ADIS16364 with Arduino

    Q: How do I connect the ADIS16364 to my Arduino processor system? --------------------------------------------------------------------------------------------- A: This software package is an example…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.