Q
I initially used the ADIS16201 in my design. I tied pins 8 and 10 to ground. Later, I redesigned my system and upgraded to the ADIS16209. Will ADIS16209 work even if pin 8 and 10 is connected to ground…
TITLE
ADIS16209 Datasheet Error: Address code length
DOCUMENT
ADIS16209 Datasheet
REVISION
E
LOCATION
Page 12 (click here), left column, first paragraph, line 8
DESCRIPTION…
Q
What is the meaning of this „R“ in the Datecode 1224R of the ADIS16209.
A
The “R” indicates that these units have had the firmware upgrade, so they would behave the same way as units with later…
Q:
Where do I find information on evaluation tools for the ADIS16209 Tilt Sensor?
----------------------------------------------------------------------------------------------------------------
…
Q
We have a problem with the self-test of ADIS16209 at power-on. Is it correct that there is a possibility to disable this function at the power-on setting the bit 10 in the register MSC_CTRL? We have…
Q:
When my ADIS16209 starts up, STATUS = 0x0020, which indicates a self-test failure, but the rest of the operation seems to be fine. Is this real? What should I do?
------------------------------…
UPDATE ALERT!
Please visit the following link for an updated set of assembly instructions:
FAQ: ADIS162xx LGA Assembly Guidelines
Start of older assembly instructions, for historical reference…
UPDATE ALERT!
Please visit the following link for an updated set of assembly instructions:
FAQ: ADIS162xx LGA Assembly Guidelines
Start of older assembly instructions, for historical reference…
Q
For my application, timing is nearly no problem. I would rotate the sensor slowly (3 rev/min) around the axis which inclination should be determined. The measured acceleration shows a sine-dependency…