ADIS16201: FAQ

Was this helpful?
  • ADIS16201 not distinguish angle (tilt) from accleration

    Q The inclinometer works very well: if I incline the device, I can measure the angles correctly. But, even if I move the device in a plain PARALLEL to the inclinometer axis, I have some variations in…
  • ADIS16201 timing between the first and second CS cycle

    Q Is it really necessary to wait 33.6us min between the first and second CS cycle when reading via the serial interface? A Yes. It's slow.
  • ADIS16201: Sample rate

    Q How does ADIS16201 generate the sample rate? How accurate is the sample rate? A The SMPL_PRD register sets the sample rate from 122us to 3.7ms and is based on an on-chip oscillator with +/-1…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.