Exporting The ADMW1001 API & Example Project

How do I export my MeasureWare project from Mbed?

  • +1
    •  Analog Employees 
    on Aug 1, 2019 2:10 AM

    If you require more advanced debugging (breakpoints, code stepping etc.) or advanced code editing/compilation it may be necessary to use a more advanced embedded IDE such as KEIL or IAR. ARM MBED provides a simple export wizard to export a program from the MBED IDE to several 3rd IDEs.

    To export a program, right click on the program folder in the “Program Workspace” and select the “Export Program” option.

    This will launch a pop up dialog where the target hardware platform and target toolchain can be selected. Clicking export will download a zip file with the exported project.