Software Examples for EV-ProMW1001ARDZ

Are there software examples available for the EV-ProMW1001ARDZ to begin development?

  • +1
    •  Analog Employees 
    on Jul 11, 2019 4:51 PM

    Analog Devices offers an API to interface to the ADMW1001 on MBED. To get up and running with the API a user has to simple drag and drop the configuration file generated in MeasureWare Designer into the MBED project and compile. The Project can be compiled for over 100 different development boards available on the MBED platform. Once the binary has been downloaded to the processor the device will begin sampling sensors based on the configuration file generated in MeasureWare designer and samples will be available through UART on the Host PC.