Please explain the two analog connectors on the EV-MW1001ARDZ

There are 4 analog channels on the ADMW1001 but only two analog connectors on the EV-MW1001ARDZ? Please explain the two analog connectors on the EV-MW1001ARDZ.

  • +1
    •  Analog Employees 
    on Jul 11, 2019 4:52 PM

    On the EV-MW1001ARDZ the analog connectors each have 1 Universal and 1 Thermocouple channels along with other pins for Power and EEPROM. This Analog connector pin definition allows a single analog board to connect to both the universal and thermocouple channel simultaneously. This enabled Thermocouple and cold junction compensation measurements on the same board when a RTD is connected to the universal channel and a Thermocouple is connected to the thermocouple channel.