The value of Gain_correction for RSSI in the Table 34 didn't show the whole condition, and it also seems like the AGC_GAIN_STATUS is not linear with the value of gain_correction.
So I'd like to ask if anyone can provide the complete table
Hello everyone,
I started studying ADF7023 for university's project. I ran into a problem: on Figure 113 show combined Single-Ended PA and LNA match,but there is no link anywhere, how to calculate capacitors and inductors. I've tried searching, but without…
Hello
I am exploring the radio module that can be used to communicate between the base and Rover gnss module with following specification.
1. Frequency range: 865 to 867MHz, unlicensed indian band.
2. Distance/ line of sight : 5km or more
3. Data rate: 58kbps…
In AN-1339, the firmware download module is for ADF7023-j.
Can I use AD_15d4 for ADF7023?