Hi,
I have able to interface ADRV9002 EVM with Arria 10 SOC EVM
I'm able to boot and initialized ADRV9002.
When i tried to connect Agro Navis 0.24.1 TES tool i was not able to connect.
any support on this.
I'm attaching you with log and screen shot of device initialization

U-Boot 2014.10-00334-gf7a7e26-dirty (Jun 30 2021 - 18:30:00), Build: jenkins-master-hdl_jobs_for_linux-projects-adrv9001.a10soc-14
CPU : Altera SOCFPGA Arria 10 Platform
BOARD : Altera SOCFPGA Arria 10 Dev Kit
I2C: ready
DRAM: WARNING: Caches not enabled
SOCFPGA DWMMC: 0
FPGA: writing socfpga_arria10_socdk.rbf ...
Full Configuration Succeeded.
DDRCAL: Success
INFO : Skip relocation as SDRAM is non secure memory
Reserving 2048 Bytes for IRQ stack at: ffe386e8
DRAM : 1 GiB
WARNING: Caches not enabled
MMC: *** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
Model: SOCFPGA Arria10 Dev Kit
Net: dwmac.ff800000
Hit any key to stop autoboot: 0
FPGA must be in Early Release mode to program core.
fpga - loadable FPGA image support
** Unable to read file u-boot.scr **
7662488 bytes read in 354 ms (20.6 MiB/s)
22104 bytes read in 14 ms (1.5 MiB/s)
FPGA BRIDGES: enable
Kernel image @ 0x010000 [ 0x000000 - 0x74eb98 ]
## Flattened Device Tree blob at 00000100
Booting using the fdt blob at 0x000100
Loading Device Tree to 01ff7000, end 01fff657 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 5.4.0-00475-gc588ee4 (jenkins@romlxbuild1.adlk.analog.com) (gcc version 9.2.0 (GCC)) #1847 SMP Fri Jul 2 09:07:42 IST 2021
[ 0.000000] CPU: ARMv7 Processor [414fc091] revision 1 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: Altera SOCFPGA Arria 10
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] cma: Reserved 128 MiB at 0x38000000
[ 0.000000] percpu: Embedded 19 pages/cpu s45196 r8192 d24436 u77824
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 260608
[ 0.000000] Kernel command line: console=ttyS0,115200 root=/dev/mmcblk0p2 rw rootwait
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 885444K/1048576K available (12288K kernel code, 1132K rwdata, 7240K rodata, 1024K init, 173K bss, 32060K reserved, 131072K cma-reserved, 131072K highmem)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] ftrace: allocating 39905 entries in 78 pages
[ 0.000000] rcu: Hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] L2C-310 erratum 769419 enabled
[ 0.000000] L2C-310 enabling early BRESP for Cortex-A9
[ 0.000000] L2C-310: enabling full line of zeros but not enabled in Cortex-A9
[ 0.000000] L2C-310 ID prefetch enabled, offset 1 lines
[ 0.000000] L2C-310 dynamic clock gating enabled, standby mode enabled
[ 0.000000] L2C-310 cache controller enabled, 8 ways, 512 kB
[ 0.000000] L2C-310: CACHE_ID 0x410030c9, AUX_CTRL 0x76460001
[ 0.000000] random: get_random_bytes called from start_kernel+0x328/0x4dc with crng_init=0
[ 0.000000] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604467 ns
[ 0.000005] sched_clock: 32 bits at 100MHz, resolution 10ns, wraps every 21474836475ns
[ 0.000013] Switching to timer-based delay loop, resolution 10ns
[ 0.000187] Console: colour dummy device 80x30
[ 0.000216] Calibrating delay loop (skipped), value calculated using timer frequency.. 200.00 BogoMIPS (lpj=1000000)
[ 0.000227] pid_max: default: 32768 minimum: 301
[ 0.000345] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)
[ 0.000358] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)
[ 0.000911] CPU: Testing write buffer coherency: ok
[ 0.000937] CPU0: Spectre v2: using BPIALL workaround
[ 0.001156] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.001661] Setting up static identity map for 0x100000 - 0x100060
[ 0.001777] rcu: Hierarchical SRCU implementation.
[ 0.002035] smp: Bringing up secondary CPUs ...
[ 0.002639] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.002645] CPU1: Spectre v2: using BPIALL workaround
[ 0.002758] smp: Brought up 1 node, 2 CPUs
[ 0.002767] SMP: Total of 2 processors activated (400.00 BogoMIPS).
[ 0.002772] CPU: All CPU(s) started in SVC mode.
[ 0.003254] devtmpfs: initialized
[ 0.006848] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[ 0.007031] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.007048] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[ 0.010942] NET: Registered protocol family 16
[ 0.012869] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.013635] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[ 0.013643] hw-breakpoint: maximum watchpoint size is 4 bytes.
[ 0.027731] vgaarb: loaded
[ 0.028014] SCSI subsystem initialized
[ 0.028183] usbcore: registered new interface driver usbfs
[ 0.028217] usbcore: registered new interface driver hub
[ 0.028264] usbcore: registered new device driver usb
[ 0.028393] usb_phy_generic soc:usbphy: soc:usbphy supply vcc not found, using dummy regulator
[ 0.029232] mc: Linux media interface: v0.10
[ 0.029269] videodev: Linux video capture interface: v2.00
[ 0.029329] pps_core: LinuxPPS API ver. 1 registered
[ 0.029334] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.029351] PTP clock support registered
[ 0.029560] jesd204: found 0 devices and 0 topologies
[ 0.029600] FPGA manager framework
[ 0.029666] Advanced Linux Sound Architecture Driver Initialized.
[ 0.030464] clocksource: Switched to clocksource timer1
[ 0.431076] NET: Registered protocol family 2
[ 0.431626] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes, linear)
[ 0.431648] TCP established hash table entries: 8192 (order: 3, 32768 bytes, linear)
[ 0.431708] TCP bind hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.431808] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.431903] UDP hash table entries: 512 (order: 2, 16384 bytes, linear)
[ 0.431946] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)
[ 0.432106] NET: Registered protocol family 1
[ 0.432517] RPC: Registered named UNIX socket transport module.
[ 0.432526] RPC: Registered udp transport module.
[ 0.432531] RPC: Registered tcp transport module.
[ 0.432536] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.432547] PCI: CLS 0 bytes, default 64
[ 0.433829] workingset: timestamp_bits=30 max_order=18 bucket_order=0
[ 0.439149] NFS: Registering the id_resolver key type
[ 0.439177] Key type id_resolver registered
[ 0.439183] Key type id_legacy registered
[ 0.439195] Installing knfsd (copyright (C) 1996 okir@monad.swb.de).
[ 0.439774] ntfs: driver 2.1.32 [Flags: R/W].
[ 0.440013] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 0.471964] bounce: pool size: 64 pages
[ 0.471979] io scheduler mq-deadline registered
[ 0.471986] io scheduler kyber registered
[ 0.476288] dma-pl330 ffda1000.pdma: Loaded driver for PL330 DMAC-341330
[ 0.476303] dma-pl330 ffda1000.pdma: DBUFF-512x8bytes Num_Chans-8 Num_Peri-32 Num_Events-8
[ 0.478711] Serial: 8250/16550 driver, 2 ports, IRQ sharing disabled
[ 0.479540] printk: console [ttyS0] disabled
[ 0.479587] ffc02100.serial1: ttyS0 at MMIO 0xffc02100 (irq = 37, base_baud = 6250000) is a 16550A
[ 1.070868] printk: console [ttyS0] enabled
[ 1.076501] brd: module loaded
[ 1.103264] spi_altera ff200040.spi: base (ptrval), irq 40
[ 1.109477] altr_a10sr_gpio altr_a10sr_gpio.0.auto: DMA mask not set
[ 1.116608] libphy: Fixed MDIO Bus: probed
[ 1.121127] CAN device driver interface
[ 1.125166] socfpga-dwmac ff800000.ethernet: IRQ eth_wake_irq not found
[ 1.131769] socfpga-dwmac ff800000.ethernet: IRQ eth_lpi not found
[ 1.138009] socfpga-dwmac ff800000.ethernet: PTP uses main clock
[ 1.144016] socfpga-dwmac ff800000.ethernet: No sysmgr-syscon node found
[ 1.150694] socfpga-dwmac ff800000.ethernet: Unable to parse OF data
[ 1.157040] socfpga-dwmac: probe of ff800000.ethernet failed with error -524
[ 1.164212] stmmaceth ff800000.ethernet: IRQ eth_wake_irq not found
[ 1.170463] stmmaceth ff800000.ethernet: IRQ eth_lpi not found
[ 1.176337] stmmaceth ff800000.ethernet: PTP uses main clock
[ 1.182130] stmmaceth ff800000.ethernet: User ID: 0x10, Synopsys ID: 0x37
[ 1.188892] stmmaceth ff800000.ethernet: DWMAC1000
[ 1.193761] stmmaceth ff800000.ethernet: DMA HW capability register supported
[ 1.200874] stmmaceth ff800000.ethernet: RX Checksum Offload Engine supported
[ 1.207976] stmmaceth ff800000.ethernet: COE Type 2
[ 1.212837] stmmaceth ff800000.ethernet: TX Checksum insertion supported
[ 1.219507] stmmaceth ff800000.ethernet: Enhanced/Alternate descriptors
[ 1.226096] stmmaceth ff800000.ethernet: Enabled extended descriptors
[ 1.232512] stmmaceth ff800000.ethernet: Ring mode enabled
[ 1.237973] stmmaceth ff800000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[ 1.253311] libphy: stmmac: probed
[ 1.256708] Micrel KSZ9031 Gigabit PHY stmmac-0:07: attached PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=stmmac-0:07, irq=POLL)
[ 1.270023] usbcore: registered new interface driver asix
[ 1.275461] usbcore: registered new interface driver ax88179_178a
[ 1.281557] usbcore: registered new interface driver cdc_ether
[ 1.287382] usbcore: registered new interface driver net1080
[ 1.293043] usbcore: registered new interface driver cdc_subset
[ 1.298952] usbcore: registered new interface driver zaurus
[ 1.304548] usbcore: registered new interface driver cdc_ncm
[ 1.310653] dwc2 ffb00000.usb: ffb00000.usb supply vusb_d not found, using dummy regulator
[ 1.318949] dwc2 ffb00000.usb: ffb00000.usb supply vusb_a not found, using dummy regulator
[ 1.327394] dwc2 ffb00000.usb: EPs: 16, dedicated fifos, 8064 entries in SPRAM
[ 1.335138] dwc2 ffb00000.usb: DWC OTG Controller
[ 1.339842] dwc2 ffb00000.usb: new USB bus registered, assigned bus number 1
[ 1.346908] dwc2 ffb00000.usb: irq 38, io mem 0xffb00000
[ 1.352346] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.04
[ 1.360589] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 1.367779] usb usb1: Product: DWC OTG Controller
[ 1.372473] usb usb1: Manufacturer: Linux 5.4.0-00475-gc588ee4 dwc2_hsotg
[ 1.379230] usb usb1: SerialNumber: ffb00000.usb
[ 1.384244] hub 1-0:1.0: USB hub found
[ 1.388008] hub 1-0:1.0: 1 port detected
[ 1.392486] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.398986] ehci-pci: EHCI PCI platform driver
[ 1.403732] usbcore: registered new interface driver uas
[ 1.409069] usbcore: registered new interface driver usb-storage
[ 1.415133] usbcore: registered new interface driver usbserial_generic
[ 1.421659] usbserial: USB Serial support registered for generic
[ 1.427658] usbcore: registered new interface driver ftdi_sio
[ 1.433400] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.440742] usbcore: registered new interface driver upd78f0730
[ 1.446649] usbserial: USB Serial support registered for upd78f0730
[ 1.454450] rtc-ds1307: probe of 0-0068 failed with error -121
[ 1.460304] i2c /dev entries driver
[ 1.464488] usbcore: registered new interface driver uvcvideo
[ 1.470208] USB Video Class driver (1.1.1)
[ 1.475732] ltc2978: probe of 0-005c failed with error -121
[ 1.481917] Synopsys Designware Multimedia Card Interface Driver
[ 1.488089] dw_mmc ff808000.dwmmc0: IDMAC supports 32-bit address mode.
[ 1.494766] dw_mmc ff808000.dwmmc0: Using internal DMA controller.
[ 1.500943] dw_mmc ff808000.dwmmc0: Version ID is 270a
[ 1.506097] dw_mmc ff808000.dwmmc0: DW MMC controller at irq 31,32 bit host data width,1024 deep fifo
[ 1.515375] mmc_host mmc0: card is polling.
[ 1.530472] mmc_host mmc0: Bus speed (slot 0) = 50000000Hz (slot req 400000Hz, actual 396825HZ div = 63)
[ 1.587139] mmc_host mmc0: Bus speed (slot 0) = 50000000Hz (slot req 50000000Hz, actual 50000000HZ div = 0)
[ 1.596885] mmc0: new high speed SDHC card at address 5048
[ 1.602846] mmcblk0: mmc0:5048 SD32G 29.7 GiB
[ 1.610083] mmcblk0: p1 p2 p3
[ 1.760472] altr_a10sr spi1.0: SPI transfer timed out
[ 1.765517] spi_master spi1: failed to transfer one message from queue
[ 1.980464] altr_a10sr spi1.0: SPI transfer timed out
[ 1.985499] spi_master spi1: failed to transfer one message from queue
[ 2.200461] altr_a10sr spi1.0: SPI transfer timed out
[ 2.205496] spi_master spi1: failed to transfer one message from queue
[ 2.420462] altr_a10sr spi1.0: SPI transfer timed out
[ 2.425497] spi_master spi1: failed to transfer one message from queue
[ 2.432235] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.438354] usbcore: registered new interface driver usbhid
[ 2.443917] usbhid: USB HID core driver
[ 2.454242] ltc2497: probe of 0-0014 failed with error -121
[ 2.460189] ltc2497: probe of 0-0016 failed with error -121
[ 2.468864] fpga_manager fpga0: SoCFPGA Arria10 FPGA Manager registered
[ 2.476137] usbcore: registered new interface driver snd-usb-audio
[ 2.483721] oprofile: no performance counters
[ 2.488151] oprofile: using timer interrupt.
[ 2.492501] drop_monitor: Initializing network drop monitor service
[ 2.499372] NET: Registered protocol family 10
[ 2.504545] Segment Routing with IPv6
[ 2.508246] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 2.514615] NET: Registered protocol family 17
[ 2.519054] NET: Registered protocol family 15
[ 2.523632] can: controller area network core (rev 20170425 abi 9)
[ 2.529828] NET: Registered protocol family 29
[ 2.534273] can: raw protocol (rev 20170425)
[ 2.538525] can: broadcast manager protocol (rev 20170425 t)
[ 2.544173] can: netlink gateway (rev 20190810) max_hops=1
[ 2.549781] 8021q: 802.1Q VLAN Support v1.8
[ 2.553991] NET: Registered protocol family 36
[ 2.558431] Key type dns_resolver registered
[ 2.562774] ThumbEE CPU extension supported.
[ 2.567030] Registering SWP/SWPB emulation handler
[ 2.596352] random: fast init done
[ 2.634700] random: crng init done
[ 11.570215] adrv9002 spi0.0: adrv9002-phy Rev 12.0, Firmware 0.16.3.8, Stream 0.7.3.0, API version: 48.8.7 successfully initialized
[ 11.583381] cf_axi_adc ff220000.axi-adrv9002-rx-lpc: ADI AIM (10.01.b) at 0xFF220000 mapped to 0x8c224a5c, probed ADC ADRV9002 as MASTER
[ 11.621096] cf_axi_dds ff22a000.axi-adrv9002-tx-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0xFF22A000 mapped to 0xf4d3625c, probed DDS ADRV9002
[ 11.635098] of_cfs_init
[ 11.637559] of_cfs_init: OK
[ 11.640530] ALSA device list:
[ 11.643485] No soundcards found.
[ 11.647067] ttyS0 - failed to request DMA
[ 11.976368] EXT4-fs (mmcblk0p2): recovery complete
[ 11.982549] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 11.990676] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 12.004593] devtmpfs: mounted
[ 12.010263] Freeing unused kernel memory: 1024K
[ 12.015105] Run /sbin/init as init process
[ 12.535812] systemd[1]: System time before build time, advancing clock.
[ 12.577606] cgroup2: Unknown parameter 'memory_recursiveprot'
[ 12.606167] systemd[1]: systemd 247.3-7+rpi1 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +ZSTD +SECCOMP +BLKID +ELFUTILS +KMOD +IDN2 -IDN +PCRE2 default-hierarchy=unified)
[ 12.629298] systemd[1]: Detected architecture arm.
Welcome to Kuiper GNU/Linux 11.2 (bullseye)!
[ 12.682030] systemd[1]: Set hostname to <analog>.
[ 14.147282] systemd[1]: /lib/systemd/system/plymouth-start.service:16: Unit configured to use KillMode=none. This is unsafe, as it disables systemd's process lifecycle management for the service. Please update your service to use a safer KillMode=, such as 'mixed' or 'control-group'. Support for KillMode=none is deprecated and will eventually be removed.
[ 14.381474] systemd[1]: Queued start job for default target Graphical Interface.
[ 14.390768] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[ 14.403095] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[ 14.412675] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 14.441396] systemd[1]: Created slice system-modprobe.slice.
[ OK ] Created slice system-modprobe.slice.
[ 14.471362] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 14.501345] systemd[1]: Created slice system-systemd\x2dfsck.slice.
[ OK ] Created slice system-systemd\x2dfsck.slice.
[ 14.531112] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 14.570967] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R…uests to Wall Directory Watch.
[ 14.600890] systemd[1]: Condition check resulted in Arbitrary Executable File Formats File System Automount Point being skipped.
[ 14.613322] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 14.640702] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 14.681684] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 14.721184] systemd[1]: Listening on fsck to fsckd communication Socket.
[ OK ] Listening on fsck to fsckd communication Socket.
[ 14.750903] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 14.802697] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
[ 14.813675] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 14.851378] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 14.889056] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 14.921156] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 14.961194] systemd[1]: Condition check resulted in Huge Pages File System being skipped.
[ 14.969788] systemd[1]: Condition check resulted in POSIX Message Queue File System being skipped.
[ 14.981717] systemd[1]: Mounting RPC Pipe File System...
Mounting RPC Pipe File System...
[ 15.013422] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 15.063154] systemd[1]: Mounting Kernel Trace File System...
Mounting Kernel Trace File System...
[ 15.100877] systemd[1]: Condition check resulted in Kernel Module supporting RPCSEC_GSS being skipped.
[ 15.117845] systemd[1]: Starting Restore / save the current clock...
Starting Restore / save the current clock...
[ 15.155827] systemd[1]: Starting Set the console keyboard layout...
Starting Set the console keyboard layout...
[ 15.190793] systemd[1]: Condition check resulted in Create list of static device nodes for the current kernel being skipped.
[ 15.205981] systemd[1]: Starting Load Kernel Module configfs...
Starting Load Kernel Module configfs...
[ 15.253670] systemd[1]: Starting Load Kernel Module drm...
Starting Load Kernel Module drm...
[ 15.293733] systemd[1]: Starting Load Kernel Module fuse...
Starting Load Kernel Module fuse...
[ 15.346636] systemd[1]: Condition check resulted in Set Up Additional Binary Formats being skipped.
[ 15.356048] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[ 15.368187] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 15.406323] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 15.421727] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 15.463571] systemd[1]: Starting Coldplug All udev Devices...
Starting Coldplug All udev Devices...
[ 15.488440] systemd[1]: Mounted RPC Pipe File System.
[ OK ] Mounted RPC Pipe File System.
[ 15.553045] systemd[1]: Mounted Kernel Debug File System.
[ OK ] Mounted Kernel Debug File System.
[ 15.591449] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Kernel Trace File System.
[ OK ] Finished Restore / save the current clock.
[ OK ] Finished Set the console keyboard layout.
[ 15.705799] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ OK ] Finished Load Kernel Module configfs.
[ OK ] Finished Load Kernel Module drm.
[ OK ] Finished Load Kernel Module fuse.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
[ OK ] Finished Remount Root and Kernel File Systems.
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
Starting Load/Save Random Seed...
[ 16.024679] systemd-journald[120]: Received client request to flush runtime journal.
Starting Apply Kernel Variables...
Starting Create System Users...
[ 16.077575] systemd-journald[120]: File /var/log/journal/f9e20e85180f46f981cb17615856faf4/system.journal corrupted or uncleanly shut down, renaming and replacing.
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Finished Load/Save Random Seed.
[ OK ] Finished Coldplug All udev Devices.
[ OK ] Finished Apply Kernel Variables.
[ OK ] Finished Create System Users.
Starting Helper to synchronize boot up for ifupdown...
Starting Create Static Device Nodes in /dev...
Starting Wait for udev To …plete Device Initialization...
[ OK ] Finished Flush Journal to Persistent Storage.
[ OK ] Finished Helper to synchronize boot up for ifupdown.
[ OK ] Finished Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
Starting Rule-based Manage…for Device Events and Files...
[ OK ] Started Rule-based Manager for Device Events and Files.
Starting Show Plymouth Boot Screen...
[ OK ] Started Show Plymouth Boot Screen.
[ OK ] Started Forward Password R…s to Plymouth Directory Watch.
[ OK ] Reached target Local Encrypted Volumes.
[ OK ] Reached target Hardware activated USB gadget.
Starting Load Kernel Module fuse...
Starting Load Kernel Modules...
[ OK ] Found device /dev/ttyS0.
[ OK ] Finished Load Kernel Module fuse.
[ OK ] Found device /dev/disk/by-partuuid/f7eeebee-01.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
Starting File System Check…isk/by-partuuid/f7eeebee-01...
[ OK ] Finished Wait for udev To Complete Device Initialization.
[ OK ] Started File System Check Daemon to report status.
[ OK ] Finished File System Check…/disk/by-partuuid/f7eeebee-01.
Mounting /boot...
[ OK ] Mounted /boot.
[ OK ] Reached target Local File Systems.
Starting Set console font and keymap...
Starting Raise network interfaces...
Starting Preprocess NFS configuration...
Starting Tell Plymouth To Write Out Runtime Data...
Starting Create Volatile Files and Directories...
[ OK ] Finished Set console font and keymap.
[ OK ] Finished Tell Plymouth To Write Out Runtime Data.
[ OK ] Finished Preprocess NFS configuration.
[ OK ] Reached target NFS client services.
[ OK ] Reached target Remote File Systems (Pre).
[ OK ] Reached target Remote File Systems.
[ OK ] Finished Create Volatile Files and Directories.
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Finished Update UTMP about System Boot/Shutdown.
[ OK ] Reached target System Initialization.
[ OK ] Started CUPS Scheduler.
[ OK ] Started Daily apt download activities.
[ OK ] Started Daily apt upgrade and clean activities.
[ OK ] Started Periodic ext4 Onli…ata Check for All Filesystems.
[ OK ] Started Discard unused blocks once a week.
[ OK ] Started Daily rotation of log files.
[ OK ] Started Daily man-db regeneration.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Paths.
[ OK ] Reached target Timers.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on CUPS Scheduler.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Listening on Erlang Port Mapper Daemon Activation Socket.
[ OK ] Listening on GPS (Global P…ioning System) Daemon Sockets.
[ OK ] Listening on triggerhappy.socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started Regular background program processing daemon.
[ OK ] Started D-Bus System Message Bus.
Starting dphys-swapfile - …unt, and delete a swap file...
Starting Remove Stale Onli…t4 Metadata Check Snapshots...
Starting Creating IIOD Context Attributes......
Starting Authorization Manager...
Starting DHCP Client Daemon...
Starting LSB: Switch to on…nless shift key is pressed)...
Starting LSB: rng-tools (Debian variant)...
Starting System Logging Service...
Starting User Login Management...
Starting triggerhappy global hotkey daemon...
Starting Disk Manager...
Starting WPA supplicant...
[ OK ] Started triggerhappy global hotkey daemon.
[ OK ] Started System Logging Service.
[ OK ] Started DHCP Client Daemon.
[ OK ] Started LSB: rng-tools (Debian variant).
[ OK ] Finished Raise network interfaces.
[ OK ] Started LSB: Switch to ond…(unless shift key is pressed).
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started Authorization Manager.
[ OK ] Started WPA supplicant.
Starting Modem Manager...
[ OK ] Reached target Network.
[ OK ] Reached target Network is Online.
Starting CUPS Scheduler...
[ OK ] Started Erlang Port Mapper Daemon.
Starting Load USB gadget scheme...
Starting HTTP based time synchronization tool...
Starting Internet superserver...
Starting /etc/rc.local Compatibility...
Starting OpenBSD Secure Shell server...
Starting Permit User Sessions...
[ OK ] Finished dphys-swapfile - …mount, and delete a swap file.
[ OK ] Started User Login Management.
[ OK ] Started /etc/rc.local Compatibility.
[ OK ] Finished Load USB gadget scheme.
[ OK ] Found device /dev/ttyGS0.
Mounting Mount FunctionFS instance...
[ OK ] Started Unattended Upgrades Shutdown.
[ OK ] Started Internet superserver.
[ OK ] Finished Permit User Sessions.
[ OK ] Mounted Mount FunctionFS instance.
Starting Light Display Manager...
Starting Hold until boot process finishes up...
[ OK ] Started HTTP based time synchronization tool.
[ OK ] Finished Remove Stale Onli…ext4 Metadata Check Snapshots.
[ OK ] Started Disk Manager.
Starting Manage, Install and Generate Color Profiles...
[FAILED] Failed to start VNC Server for X11.
Raspbian GNU/Linux 11 analog ttyS0
analog login: root (automatic login)
Linux analog 5.4.0-00475-gc588ee4 #1847 SMP Fri Jul 2 09:07:42 IST 2021 armv7l
The programs included with the Debian GNU/Linux system are free software;
the exact distribution terms for each program are described in the
individual files in /usr/share/doc/*/copyright.
Debian GNU/Linux comes with ABSOLUTELY NO WARRANTY, to the extent
permitted by applicable law.
Last login: Thu Aug 4 16:17:12 BST 2022 on ttyS0
root@analog:~#
root@analog:~#
--
Regards
Vivek V