Post Go back to editing

ADF7021 application components

Hi everyone. I am in charge of designing a communication system with the ADF7021 transceiver. It will operate at a frequency close to 430 MHz. In the EVAL-ADF7021DBZX data sheet it is mentioned that the EVAL-ADF7021DBZ3 evaluation board works in the frequency range of 431 MHz to 470 MHz and the values corresponding to the components with the ones that the board works in this range, but is there somewhere explained a way in which those values can be obtained with an equation? Or how could you tune those values to work on a certain frequency?