In AN-1339, the firmware download module is for ADF7023-j.
Can I use AD_15d4 for ADF7023?
ADF7023
Not Recommended for New Designs
The ADF7023 is a very low power, high performance, highly integrated 2FSK/GFSK/OOK/MSK/GMSK transceiver designed for operation in the 862 MHz to 928 MHz...
Datasheet
ADF7023 on Analog.com
ADF7023-J
Not Recommended for New Designs
The ADF7023-J is a very low power, high performance, highly integrated 2FSK/GFSK/MSK/GMSK transceiver designed for operation in the 902 MHz to 958 MHz...
Datasheet
ADF7023-J on Analog.com
In AN-1339, the firmware download module is for ADF7023-j.
Can I use AD_15d4 for ADF7023?
Hi,
Yes. AD_15d4 should also work for ADF7023.
Regards,
Aldrich