Where can I get the firmware download for image rejection calibration?

Where can I get the image rejection calibration firmware download? How do I run it?

Parents
  • 0
    •  Analog Employees 
    on Jul 23, 2014 3:49 PM

    The image rejection calibration firmware download is included with the ADF7024 design resource package, which can be found on the ADF7024 product page at www.analog.com/adf7024.  For details on the IR calibration algorithm and firmware download, please refer to application note AN-1315: Autonomous IR Calibration on the ADF7024, also available as part of the ADF7024 design resource package.

    The ADF7024 Evaluation GUI can also be used to perform and evaluate the IR calibration.

Reply
  • 0
    •  Analog Employees 
    on Jul 23, 2014 3:49 PM

    The image rejection calibration firmware download is included with the ADF7024 design resource package, which can be found on the ADF7024 product page at www.analog.com/adf7024.  For details on the IR calibration algorithm and firmware download, please refer to application note AN-1315: Autonomous IR Calibration on the ADF7024, also available as part of the ADF7024 design resource package.

    The ADF7024 Evaluation GUI can also be used to perform and evaluate the IR calibration.

Children
No Data