Running the ADF7024 from the ADuCM3029 board using IAR?

I would like to run the ADF7024 from the ADuCM3029 eval board. I have IAR installed, should I use that, is there example code available?

  • 0
    •  Analog Employees 
    on Jul 4, 2016 3:10 PM

    Hi

    Apologies for the delay in replying to this. The ADF7024 is hardware compatible with the ADuCM3029 board as it has the connector for the ADF7024 daughter boards. From a software point of view we don't have any example code for using the ADF7024 with the ADuCM3029. However it should be possible to set this up using the ADuCM302x EZ-KIT BSP for IAR (Rev. 1.0.1) package as a starting point. See this link to download the BSP package. We do provide example embedded code for the ADF7024 but is based on the Renesas RL78 MCU as that is the Host MCU used on the ADF7xxxMB4Z mother board.

    Regards

    Conor

  • Where can I find example embedded code for the ADF7024, based on the Renesas RL78 MCU for the ADF7xxxMB4Z mother board?