Post Go back to editing

ooking for COTS RF Evaluation Board to Transmit/Receive 100 kHz PWM Signal at 60 GHz

Category: Hardware

I am looking for a COTS RF evaluation board that includes a built-in MCU, transceiver, and antenna. The device should be capable of transmitting a 100 kHz PWM signal over a 60 GHz RF transceiver. Another transceiver should be able to receive the signal and convert it back into PWM. These devices will be placed close to each other. I have researched several evaluation boards, but I have been unable to confirm if they can support this setup, as I am new to RF technology. If 60 GHz is not feasible, a 5.8 GHz solution would also work.