Hi,
The datasheet of MAX7044 says "The crystal oscillator in the MAX7044 is designed to present a capacitance of approximately 3pF between the XTAL1 and XTAL2 pins." That means there are an extra 3pF load capacitor internal the chip, right? And it won't prevent me to use external load capacitors, if I use a crystal with larger load capacitor, I need use external load capacitors, right?
Thanks.
Edit Notes
Review[edited by: diverger at 10:52 AM (GMT -4) on 23 Apr 2024]