Post Go back to editing

ADF7241 SPI RC_READY bit getting stuck at 0

Hello all,


I am working on a driver for the ADF7241/ADF7242 radio and during my testing I'm finding the RC_READY bit from the SPI status word is sometimes getting stuck at 0. The register dump when this occurs looks like this:

0x630: b80f92c80f971c0f955b16161f000505 02000000000000000000000000000000
0x100: 0000080000c4000134c0c000317aaa18 7a0b2e310000aaaaaaaaaaaaaaaa0f1a
0x120: 534700bb770fbf8f2f563bb3dbb1babf 0b0500ca8922b7f90000610a0d080003
0x300: 20b903053206014000060100c3004e20 00000000800000000000000800b80703
0x320: 83bb0000000242720000000000000000 000000000017020f031f0f0c0f3c4000
0x340: 00000421098000101609002100013f00 961c1800000821130000000000000100
0x360: 00000000000000000000001b013f6f09 0720020ff001001a0400f10000000000
0x380: 384b1b1f00000100000504ff25141000 00000000840008000260801d00000002
0x3a0: 001d2409100000074d00f10909010000 00103000906d2e2318132d1579020002
0x3c0: 22222200050000001a0200c86a00ff00 10821b1a020302000100000000000000
0x3e0: f2080000a30100000000000000000400 20005a05a70000000000008d6b0208b4

The driver is set up to write RC_RESET (0xC8) to the SPI when this occurs, but I find that this causes more problems. The RC_READY bit gets stuck regularly under normal usage of the radio and I would like to figure out what is happening if possible. What could I do to debug this issue?

Thanks