Please advise ADF7030-1 Supports which topology ex:star,Mesh etc.,

we are planning to develop a Sub-GHz module for AMR and Meter Applications.. and it should support Star topology and also please advise how many nodes we can connect with same device..??

Please advise can ADF7030-1 can supports for the same..

Parents
  • yes the ADF7030-1 supports a mesh topology. There isn't an absolute limit to the number of end points that can be supported rather a practical limit based upon how often each end point will need to communicate with the base and the message length and datarate. For example if each node sends a 1ms message once a second then the limit would be 1000. If a message were sent every minute then significantly more nodes could be supported.

Reply
  • yes the ADF7030-1 supports a mesh topology. There isn't an absolute limit to the number of end points that can be supported rather a practical limit based upon how often each end point will need to communicate with the base and the message length and datarate. For example if each node sends a 1ms message once a second then the limit would be 1000. If a message were sent every minute then significantly more nodes could be supported.

Children
No Data