ADF5355
Recommended for New Designs
The ADF5355 allows implementation of fractional-N or integer-N phase-locked loop (PLL) frequency synthesizers when used with an external loop filter and...
Datasheet
ADF5355 on Analog.com
Hi all,
I'm not seeing ADF5355 driver in Raspberry pi kernel (https://github.com/raspberrypi/linux ). I tried versions up to 4.16.
Under Synthesizers DDS/PLL category, I can see only ADF4350/ADF4350 as shown below :
Also, ADF5355 IIO Wideband Synthesizer Linux Driver [Analog Devices Wiki] suggests to set the following options.
--- Industrial I/O support -*- Enable ring buffer support within IIO -*- Industrial I/O lock free software ring -*- Enable triggered sampling support
but what I get is as follows : There's no option for "Enable ring buffer support" & "Industrial I/O lock free software ring"
I saw this post : Stuck setting up ADF5355 and it says ADF5355 is working with Raspberry Pi3, but the post does not tell the steps taken to install the driver. I don't know much about kernel/driver installation & I don't know where to put .dts files, where to put source files (.h .c) etc. when adding new drivers.
Please bare with me, my linux kernel/driver installation knowledge is very limited.
It would be great if someone could guide me to control ADF5355 with RPi 3 using iio device driver.
Cheers,
I don't think there is a overlay for the ADF5355.
Simply copy this linux/rpi-adxl372-overlay.dts at rpi-4.9.y · analogdevicesinc/linux · GitHub
and add the example from here: ADF5355 IIO Wideband Synthesizer Linux Driver [Analog Devices Wiki]
-Michael
hello sir I want to know to make the health sensor max30100 work .
I tried so hard to find a solution but I couldn't.
thanks.
hello sir I want to know to make the health sensor max30100 work .
I tried so hard to find a solution but I couldn't.
thanks.
Please stop posting random queries.
This is a support community for Analog Devices IC.
Sorry sir, I just needed some help this is the only platform that I found could help me.
thanks snd sorry.