Is there a patch available for device tree support for the AD5933? This was referenced in November 2017 in the post below.
We are generating the MCLK input to the AD5933 using direct digital synthesis, as suggested in the AD5933 datasheet, as we need to measure at frequencies lower than what the internal oscillator will allow for. And for our application, we need to be able to change the external clock frequency. I don't presently see any way to do that with the current driver.