Post Go back to editing

ADRV9371 evaluation software spurious signals

Thread Summary

The user encountered spurious signals when using the AD9371 IIO OSC software with a 2550 MHz center frequency and a 2560 MHz input signal. The issue was resolved by updating the kernel package to a newer version, which eliminated the spurious signals at both 61.44 MSPS and 122.88 MSPS sample rates. The AD9371 Filter Wizard settings were also reviewed, but the core problem was related to the kernel and device driver configuration.
AI Generated Content

Hello Team,

I have an ADRV9371-W/PCBZ card from Analog Devices.

I use the AD9371 IIO OSC software, and there is a problem.I set the center frequency of the receiving channel to 2550MHz,and connect a single tone signal of 2560MHz,Why are there so many spurious signals?Is there a problem with my setting?How should I set it up?

and I use the "Wide Tuning Range AD9371 Eval Brd Transceiver Evaluetion Software" is OK.

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.