ADAU1372 on Beaglebone Black

I'm trying to compile the ADAU1372 modules for the Beaglebone Black and not having much luck.  I noted that the supposedly mainlined ADAU1373 didn't pop up as an option in my menuconfig, either, so I figured I finally needed to ask folks here as I'm clearly not doing something right.

To compile, I do the following (I'm on Ubuntu 16.10, but that shouldn't be that important since this is a cross compile):

git clone github.com/.../ti-linux-kernel-dev.git
cd ti-linux-kernel-dev
git checkout tags/4.4.54-ti-r93
git checkout -b 4.4.54-ti-r93-adau1372
./build_kernel.sh

After letting that grind away a bit and getting all of the prerequisites downloaded, a "make menuconfig" window pops up.  When I go down into "Device Drivers"->"Sound card support"->"Advanced Linux Sound Architecture"->"ALSA for SoC audio support"->"CODEC drivers"  I see that neither the ADAU1372 that I tried to add nor the ADAU1373 which is supposed to be mainlined are present.

Where and how do I add the adau1372 modules in order to get them to compile?

Thanks.

Parents Reply Children
No Data