Post Go back to editing

Need help to resolve the failures in digital tuning of the AD-FMCOMMS3-EBZ (AD9361 Transceiver) channels

Hi guys,

     We are developing customized AD-FMCOMMS3-EBZ board.

     We are encountering with problem in digital tuning the both Tx Channel and Rx channel during booting up of the linux in CMOS mode.

     We are getting the following messages during Linux kernel boot up.

     SAMPL CLK: 61440000 tuning: RX

       0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:

     0:# # # # # # # # # # # # # # # #

     1:# # # # # # # # # # # # # # # #

     ad9361 spi32766.0: ad9361_dig_tune: Tuning RX FAILED!

     SAMPL CLK: 61440000 tuning: TX

       0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:

     0:# # # # # # # # # # # # # # # #

     1:# # # # # # # # # # # # # # # #

     ad9361 spi32766.0: ad9361_dig_tune: Tuning TX FAILED!

     cf_axi_adc: probe of 79020000.cf-ad9361-lpc failed with error -5

     Basically, we are not able to see any data transfers to and from the customized board after the customized board is booted up.

     Can anybody guide us as to how we can resolve the issues in digital tuning both Tx and Rx channels?

     Can anybody summarize the steps to be followed to trouble-shoot the issues related to digital tuning of the channels?

     Thanks in advance.

Parents
  • We're using LVDS and are running on an RTOS so we're using a .c as our config. I tried setting swap_ports_enable to 1 but it did not work.

    Can you please let me know if what I am seeing is correct, during the digital loopback part of ad9361_dig_tune() when TX is being calibrated, should adc_valid be asserting twice as often as dac_valid?

Reply
  • We're using LVDS and are running on an RTOS so we're using a .c as our config. I tried setting swap_ports_enable to 1 but it did not work.

    Can you please let me know if what I am seeing is correct, during the digital loopback part of ad9361_dig_tune() when TX is being calibrated, should adc_valid be asserting twice as often as dac_valid?

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.