I am currently working with the ZCU102 and AD9081 using the ad9081_fmx_ebz reference design. The base project is configured for a 61.44 MSPS sample rate for both the Tx and Rx JESD204 datapaths. the project has been created on petalinux.
To support my specific waveform requirements, I have modified the HDL design with the following two changes:
-
Resampling: Added an Interpolation-by-4 block in the Tx path and a Decimation-by-4 block in the Rx path.
-
Data Offload: Configured both the Tx and Rx data offload blocks to operate in bypass mode.
The Issue: I am streaming data from the PC to the Tx path at 15.36 MSPS (which interpolates to 61.44 MSPS at the DAC). I am looping this back into the Rx path, where it is decimated back down by 4. I expect to receive the data at the PC at exactly 15.36 MSPS. However, I am experiencing data loss on the Rx side, resulting in an observed data rate that is lower than 15.36 MSPS. one more thing i want to mention that at board level using same application the data throughput coming exactly 15.36Msps. then why there is loss at PC level.