Post Go back to editing

Constraints

Thread Summary

The user asked about the meaning and necessity of specific CMOS clock latency constraints (2 ns early, 5 ns late) for the ADRV9001 on a Zedboard. The final answer explains that these values account for PCB trace delays and component propagation delays, and advises recalculating these values for a custom board. The accompanying answer clarifies that these constraints ensure the design meets setup and hold timing requirements.
AI Generated Content
Category: Hardware
Product Number: adrv9001

In the example project of ADRV9001 for zedboard, the CMOS constraint file have the following constraint. 

set_clock_latency -source -early 2 [get_clocks rx1_dclk_out]
set_clock_latency -source -early 2 [get_clocks rx2_dclk_out]

set_clock_latency -source -late 5 [get_clocks rx1_dclk_out]
set_clock_latency -source -late 5 [get_clocks rx2_dclk_out]

Can someone explain these? Also, do I need to add these on my project?
I am using adrv9001 on a custom board with a Zynq7000 soc. 

Thread Notes

Parents
  • The values of 2 and 5 ns (early and late corners) have been calculated by taking into account the real physical lengths of the PCB traces as well as any delays introduced by other components on the signal path. For your custom board you need to calculate the PCB trace delay (depends on the type of dielectric used in the PCB, typically ~6 inches/ns in FR4) and the component propagation delay for components sitting on the signal path, you should find this information in the datasheets of the components you used.

Reply
  • The values of 2 and 5 ns (early and late corners) have been calculated by taking into account the real physical lengths of the PCB traces as well as any delays introduced by other components on the signal path. For your custom board you need to calculate the PCB trace delay (depends on the type of dielectric used in the PCB, typically ~6 inches/ns in FR4) and the component propagation delay for components sitting on the signal path, you should find this information in the datasheets of the components you used.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.