Post Go back to editing

How to add ad9364 in between my custom Transmitter and Receiver?

Thread Summary

The user is designing a custom BPSK/QPSK transmitter and receiver for a ZedBoard + FMCOMMS4 setup, with 12-bit I/Q data. The solution involves integrating the custom design directly into the `axi_ad9361` datapath without using DMA for sample transfer, and handling the 12-bit to 16-bit data interface conversion. The user should also address clock domain crossing (CDC) issues by using FIFO generators to synchronize data between the 16.384 MHz custom design and the AD9364's different clock domains.
AI Generated Content
Category: Hardware

I'm using a zedboard + fmcomms4 setup. So, I'm designing a custom BPSK/QPSK transmitter and receiver. I have constructed the Tx and Rx hierarchy in vivado block design. The Tx outputs 12 bits I/Q and the Rx has 12 bits inputs I/Q. The confusion is how do I insert the ad9361 (so as to transmit and receive those I/Q samples over the air). Should I connect the relevant DAC and ADC ports on axi_ad9361 module or use the ADC/DAC DMA? I wish to access the Tx-Rx design via kuiper linux (installed on the sd card) terminal (with Putty) and run python scripts to check if the transmitter/receiver is working and what is the bit error rate, etc.

Thread Notes

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.