Post Go back to editing

ADI Linux 6.12 2026R2 – Release Timing and Upstream Kernel Version

Thread Summary

The user inquires about the ADI Linux 6.12 2026R2 release plan, specifically the expected availability and the upstream Linux version it will be based on. The final answer confirms that the 2026R2 release is planned for November-December 2026 and will be based on a version of the upstream Linux 6.12.x, but does not specify if it will be 6.12.94 or later. The 2026R1 release is based on upstream Linux 6.12.77.
AI Generated Content
Category: Software
Product Number: Kernel
Software Version: 6.12.0

Hi,

I would like to understand ADI’s release plan for the Linux 6.12 LTS kernel, specifically the upcoming 2026R2 release.

My understanding is that:

  • ADI 2026R1 was originally based on upstream Linux 6.12.77.
  • There is now an ADI branch named xlnx/release/v6.12.y-2026r1-94, which appears to be based on upstream Linux 6.12.94.

Could you please clarify the following?

  1. When is the ADI Linux 6.12 2026R2 release expected to be available?
  2. What upstream Linux 6.12.x version will 2026R2 be based on?
    • Will 2026R2 be based on 6.12.94, similar to the current 2026r1-94 branch?
    • Or is a newer upstream 6.12 LTS baseline planned for R2?
  3. In particular, when does ADI expect to provide a Linux 6.12 release based on upstream Linux 6.12.97 or later?
Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.