Post Go back to editing

Linux Support for ADRV9029 CFR and DPD

Thread Summary

The user is experiencing issues with the ADRV9025 DPD engine calibrations and ORX channel mapping on a Zynq Ultrascale+ MPSoC. Despite setting orxEnableMode to ADI_ADRV9025_ORX_EN_SINGLE_CH_2PIN_MODE in ActiveUtilInit.profile, the driver still expects the orx_to_tx_mapping attributes to be set. The final answer indicates that this is a duplicate question and directs the user to an existing thread for further discussion.
AI Generated Content
Category: Software
Product Number: ADRV9029

Dear team,

On our custom hardware which has Zynq Ultrascale plus MPSoC and ADRV9025, we are using 13-NLS profile with ORX.
HDL built over Vivado 2025.1 and Petalinux over 2025.1 environment.

We are trying to run the DPD engines for all the four TX channels, with ORX mapping to be TX1 and TX2 for ORX1 & ORX3 for TX3 and TX4.

We have changed the orxEnableMode to ADI_ADRV9025_ORX_EN_SINGLE_CH_2PIN_MODE in the ActiveUtilInit.profile, as shown below:

"radioCtrlInit": {

"orxRadioCtrlModeCfg": {

        "orxEnableMode": 2,

        "orxPinSelectSettlingDelay_armClkCycles": 15,

        "singleChannel1PinModeOrxSel": 4,

        "singleChannel2PinModeLowOrxSel": 0,

        "singleChannel2PinModeHighOrxSel": 2,

        "dualChannel2PinModeOrxSel": 4

      }

}

Each of the signals, orx_control_enable_a, orx_control_enable_b, orx1_tx_sel, and orx3_tx_sel are controlled through the GPIOs.

  1. While running the calibrations for ext_path_delay and ext_tx_lol, the driver still expects the debugfs attribute orx1_to_tx_mapping and orx3_to_tx_mapping to be set to corresponding TX channel mapped to. If not mapped correctly it is throwing error "Invalid Tx channel selected".
  2. Also while switching the TX channels during DPD run, we have to switch the GPIO as well as set the orx_to_tx_mapping attribute. Only switching the GPIO is providing data of wrong path to the DPD engine to correct.

It seems that the orxEnableMode is still set in ADI_ADRV9025_ORX_EN_SPI_MODE even though modified the ActiveUtilInit.profile.

How can we acknowledge that the orxEnableMode has been set to the intended mode in the driver ?

Thanks and regards,

Satyam

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.