Post Go back to editing

PETALINUX IMAGE OFFLINE BUILD FAILED

Category: Software
Product Number: AD-JUPITER-EBZ
Software Version: 2025_R1

Hi,

I am using AD-JUPITER-EBZ board. I am using VIVADO 2025_R1  and Petalinux 2025_R1.I have downloaded https://github.com/analogdevicesinc/hdl and created project.

I have created petalinux image by following the steps https://github.com/analogdevicesinc/meta-adi/blob/main/meta-adi-xilinx/README.md . Image is working but now I need to create Image without internet.

I have tried the procedure https://xilinx-wiki.atlassian.net/wiki/spaces/A/pages/60129817/Xilinx+Yocto+Builds+without+an+Internet+Connection but I am getting error


$ bitbake -c fetchall petalinux-image-minimal
ERROR: The following layer directories do not exist:
ERROR: /home/digital_c2r/karthik/ad_jupiter_ebz/components/yocto/layers/poky/meta-yocto-bsp
ERROR: Please check BBLAYERS in /home/digital_c2r/karthik/ad_jupiter_ebz/components/yocto/layers/poky/build/conf/bblayers.conf

I am attaching a file contains sequence of steps I have followed.

I need the complete procedure to create petalinux image without internet.

 

digital_c2r@DIGITALC2R:~/karthik$ source /tools/peta/settings.sh
*************************************************************************************************************************************************
The PetaLinux source code and images provided/generated are for demonstration purposes only.
Please refer to https://xilinx-wiki.atlassian.net/wiki/spaces/A/pages/2741928025/Moving+from+PetaLinux+to+Production+Deployment
 for more details
*************************************************************************************************************************************************
PetaLinux environment set to '/tools/peta'
[INFO] Checking free disk space
[INFO] Checking installed tools
[INFO] Checking installed development libraries
[INFO] Checking network and other services
[WARNING] No tftp server found - please refer to "UG1144 2025.1 PetaLinux Tools Documentation Reference Guide" for its impact and solution
digital_c2r@DIGITALC2R:~/karthik$ petalinux-create project --template zynqMP -n ad_jupiter_ebz
[INFO] Create project: ad_jupiter_ebz
[INFO] New project successfully created in /home/digital_c2r/karthik/ad_jupiter_ebz
digital_c2r@DIGITALC2R:~/karthik$ cd ad_jupiter_ebz
digital_c2r@DIGITALC2R:~/karthik/ad_jupiter_ebz$ petalinux-config --get-hw-description=/home/digital_c2r/karthik/ad_jupiter_ebz
[INFO] Getting hardware description
[INFO] Renaming system_top.xsa to system.xsa
[INFO] Extracting yocto SDK to components/yocto. This may take time!
[INFO] Bitbake is not available, some functionality may be reduced.
[INFO] Using HW file: /home/digital_c2r/karthik/ad_jupiter_ebz/project-spec/hw-description/system.xsa
[INFO] Getting Platform info from HW file
[INFO] Generating Kconfig for project
[INFO] Menuconfig project
[INFO] Generating kconfig for rootfs
[INFO] Silentconfig rootfs
[INFO] Generating configuration files
[INFO] Adding user layers
[INFO] Generating machine conf file
[INFO] Generating plnxtool conf file
[INFO] Generating workspace directory
NOTE: Starting bitbake server...
NOTE: Started PRServer with DBfile: /home/digital_c2r/karthik/ad_jupiter_ebz/build/cache/prserv.sqlite3, Address: 127.0.0.1:36127, PID: 2347651
INFO: Specified workspace already set up, leaving as-is
INFO: Enabling workspace layer in bblayers.conf
[INFO] Successfully configured project
digital_c2r@DIGITALC2R:~/karthik/ad_jupiter_ebz$ cd components/yocto/layers/poky/
digital_c2r@DIGITALC2R:~/karthik/ad_jupiter_ebz/components/yocto/layers/poky$ source oe-init-build-env
You had no conf/local.conf file. This configuration file has therefore been
created for you from /home/digital_c2r/karthik/ad_jupiter_ebz/components/yocto/layers/poky/meta-poky/conf/templates/default/local.conf.sample
You may wish to edit it to, for example, select a different MACHINE (target
hardware).

You had no conf/bblayers.conf file. This configuration file has therefore been
created for you from /home/digital_c2r/karthik/ad_jupiter_ebz/components/yocto/layers/poky/meta-poky/conf/templates/default/bblayers.conf.sample
To add additional metadata layers into your configuration please add entries
to conf/bblayers.conf.

The Yocto Project has extensive documentation about OE including a reference
manual which can be found at:
    https://docs.yoctoproject.org

For more information about OpenEmbedded see the website:
    https://www.openembedded.org/

This is the default build configuration for the Poky reference distribution.

### Shell environment set up for builds. ###

You can now run 'bitbake <target>'

Common targets are:
    core-image-minimal
    core-image-full-cmdline
    core-image-sato
    core-image-weston
    meta-toolchain
    meta-ide-support

You can also run generated qemu images with a command like 'runqemu qemux86-64'.

Other commonly useful commands are:
 - 'devtool' and 'recipetool' handle common recipe tasks
 - 'bitbake-layers' handles common layer tasks
 - 'oe-pkgdata-util' handles common target package tasks
digital_c2r@DIGITALC2R:~/karthik/ad_jupiter_ebz/components/yocto/layers/poky/build$ cd ../../../
digital_c2r@DIGITALC2R:~/karthik/ad_jupiter_ebz/components/yocto$ cd ../../
digital_c2r@DIGITALC2R:~/karthik/ad_jupiter_ebz$ bitbake -c fetchall petalinux-image-minimal
ERROR: The following layer directories do not exist:
ERROR:    /home/digital_c2r/karthik/ad_jupiter_ebz/components/yocto/layers/poky/meta-yocto-bsp
ERROR: Please check BBLAYERS in /home/digital_c2r/karthik/ad_jupiter_ebz/components/yocto/layers/poky/build/conf/bblayers.conf
digital_c2r@DIGITALC2R:~/karthik/ad_jupiter_ebz$

Thread Notes

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.