KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADRV9002
Recommended for New Designs
The ADRV9002 is a highly integrated RF transceiver that has dual-channel transmitters, dual-channel receivers, integrated synthesizers, and digital signal...
Datasheet
ADRV9002 on Analog.com
Hi,
Currently i am trying to establish a ADC DAC loopback for ADRV9002 transceiver for ZCU102 eval board. For that i have taken the HDL and C files from the github and make changes in it as per the requirement . While doing so i am facing some error messages on launching the project. The issue is very frequent and i got stuck into it. I have attached the prints of the error, kindly look into it and suggest any changes or modification in the project if required. Also let me know if any further information you required so as to establish the loopback.
regards,
Anurag
Hello [ERROR]: Error number 3 (0x00000003), Recovery action -101.In file ../noos/drivers/rf-transceiver/navassa/devices/adrv9001/public/src/adi_adrv9001_arm.c, in function adi_adrv9001_arm_CmdStatus_Wait, in line 671, variable name device.Error message ArmCmdStatusWait() failed due to thrown ARM error. Is device in correct state for calling command?. [ERROR]: Error number 13315 (0x00003403), Recovery action -2.In file ../noos/drivers/rf-transceiver/navassa/devices/adrv9001/private/src/adrv9001_arm.c, in function adrv9001_ArmCmdErrorHandler, in line 2852, variable name mailboxErrCode.Error message Error occurred during an Init Calibration. Check that no signal is being applied to the Rx ports. Check that correct external LOs are applied, and synchronized, where appropriate. [ERROR]: Error number 13315 (0x00003403), Recovery action -2.In file ../noos/drivers/rf-transceiver/navassa/devices/adrv9001/public/src/adi_adrv9001_cals.c, in function adi_adrv9001_cals_InitCals_Run, in line 117, variable name NULL.Error message Error occurred during an Init Calibration. Check that no signal is being applied to the Rx ports. Check that correct external LOs are applied, and synchronized, where appropriate. adrv9002_setup, 981: failed with "Error occurred during an Init Calibration. Check that no signal is being applied to the Rx ports. Check that correct external LOs are applied, and synchronized, where appropriate" (13315)
RahulMushini - Moved from Support ADRV9001 – ADRV9007 to Linux Software Drivers. Post date updated from Thursday, May 21, 2026 10:21 AM UTC to Thursday, May 21, 2026 12:57 PM UTC to reflect the move.
RahulMushini - Moved from Support ADRV9001 – ADRV9007 to Linux Software Drivers. Post date updated from Thursday, May 21, 2026 12:57 PM UTC to Thursday, May 21, 2026 12:57 PM UTC to reflect the move.
Hello! We will close this thread since it is a duplicate of the following one: (+) Issues in ADC DAC loopback for ADRV9002 transceiver for ZCU102 eval board - Q&A - Linux Software Drivers - EngineerZone.
Please follow that thread for further updates.