Post Go back to editing

adrv904x with vck190

Thread Summary

The user inquired about the availability of HDL support for the ADRV904x with the VCK190 development board. The final answer explains that due to the hardware incompatibility (VCK190 supplies 1.5V while ADRV904x requires 1.8V), support for this combination is not available. The only supported configurations are ADRV9026 with VCK190 and ADRV904x with ZCU102.
AI Generated Content
Category: Hardware
Product Number: ADRV9042

Hi,

I have seen there is a branch https://github.com/analogdevicesinc/linux/tree/adrv904x_vck190 for the adrv904x with the cvk190 development board for the linux part but looking in the hdl repo didn't found any version compatible with this combination.

why?

At least the only versions/branches for the vck190 you provide are for the adrv9026 and for the adrv904x I can only find the zcu102 project.

I would like to use this combination, could you provide the guidelines?.

Thanks,

regards.

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.