Post Go back to editing

AD9371+ zcu102

Thread Summary

The user is trying to bring up the ADRV9371 on a ZCU102 platform using a bitstream generated with Vivado 2024.2. The final answer suggests building the device tree, kernel, and BOOT.bin manually, as meta-adi does not support PetaLinux 2024.2. The user should verify device initialization and data path functionality. The accompanying answers clarify that using a 2023 PetaLinux image with a 2024.2 bitstream is not recommended and ask for the desired sample rate and JESD mode.
AI Generated Content
Category: Software
Product Number: AD9371

Hi ,

I have a using ADRV9371, i have gebnerated build for zcu102 fpga board from ADI hdl git repo with 2024.2 Vivado version, after generating bit file 

1. What is the next step to get ADC / DAC data and configure sampling rate of Transciever?

2. If we will download Petalinx imagae for IIO etc then how to control / process data further in PL side of FPGA ?

3. My build bit file is generated with repect to 2024.2 Vivado version so can i work with petalinux image that is om 2023 by ADI?

Please assist for the same.

Thread Notes

Parents
  • 2. If we will download Petalinx imagae for IIO etc then how to control / process data further in PL side of FPGA ?

    Not sure what you mean by this?

    3. My build bit file is generated with repect to 2024.2 Vivado version so can i work with petalinux image that is om 2023 by ADI?

    If you mean using meta-adi 2023_R2, that supports petalinux 2023.2 so it is likely not a good idea to use a bitstream using 2024.2. Might work but we can't really give any support if it does not work.

    - Nuno Sá

Reply
  • 2. If we will download Petalinx imagae for IIO etc then how to control / process data further in PL side of FPGA ?

    Not sure what you mean by this?

    3. My build bit file is generated with repect to 2024.2 Vivado version so can i work with petalinux image that is om 2023 by ADI?

    If you mean using meta-adi 2023_R2, that supports petalinux 2023.2 so it is likely not a good idea to use a bitstream using 2024.2. Might work but we can't really give any support if it does not work.

    - Nuno Sá

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.